This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ14203H: LMZ14203: LMZ14203H Startup Problem

Part Number: LMZ14203H

Tool/software:

I have a very strange problem with the circuit in the attached drawing.

The Vin is 18-30VDC, nominal 24VDC and the required output Vo 14.2V.

The UVLO is set at 16.2V. Output capacitors are all ceramicThe load is linear at 350mA.

What happens is that when I apply +24VDC  the output voltage is only about 6V with a high ripple.

Also, it apparently overloads the input protection circuit (not shown in the drawing).

If I quickly disconnect the power and connect again it works normally.

At 28V it does the same but it won't start no matter how many times I switch the power on/off.

But at 20V it works normally, starts every time at the working parameters.

I am working with the LMZ a lot in many products, same circuit and never had such a phenomena.

The only thing changed in this circuit are the output capacitors, I used so far tantalum and here I changed to ceramic, same value. 

I will appreciate any help.