Other Parts Discussed in Thread: BQ25887
Tool/software:
Hi,
I have few questions regarding BQ25886RGER.
- What will be the SYS voltages if single cell lipo max voltages are 4.2V i.e. Total 8.4V
- Is SYS voltages are regulated or simply BAT voltages?
- There are two pin name for pin1 on the datasheet. Which one is correct?
- I want to use this charger in standalone mode. Can i leave pins 24,1,5, and 3 NC?
- I don't have battery thermistor neither i want to use any. Can i leave NC this pin