This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61169: Recommendation for suitable IR LED driver

Part Number: TPS61169
Other Parts Discussed in Thread: TPS923652

Tool/software:

Hi Team, 

I have a design challenge due to the provision in the product design to allow users to change LED brightness. 

Below is the IR led VI characteristic, user will be able to change Led forward current(If)  from 40mA to 400mA,   With Vin=5V, which LED driver would you recommend? 
If Total Vf
40mA 3.6V
80mA 4.06V
100mA 4.3V
120mA 4.58V
140mA 4.8V
160mA 5.0V
180mA 5.2V
200mA 5.4V
300mA 5.8V
400mA 6.0V

Regards,

James