Part Number: TPS25200
Other Parts Discussed in Thread: TPS25947, TPS2552, TPS2661, TPS2640, TPS2662
Tool/software:
Hi,
We are using the TPS25200 eFuse with reverse current blocking in our product design. However, there are instances when the current may flow in the reverse direction, from the output to the input, while the TPS25200 is powered off. This can happen if the user mistakenly connects to the output of the TPS25200 instead of the input.
In such cases, we have observed that the TPS25200 overheats and fails.
Could you recommend alternative components/parts/products that would allow current to flow from the output to the input while protecting the TPS25200? Adding a Schottky diode in series with the output is not a viable option due to the voltage drop across the diode. Our maximum output voltage is 5.5V, and the output current is 150mA.
Thank you.