This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80: Set FTEMP 0 or 1?

Part Number: BQ40Z80

Tool/software:

What is the different between set FTEMP 0 or 1?

1 = average

0 = Max

Is this about the ADC filter?

Please give me a example. Thanks you very much.

  • Hi Xavier,

    The difference between the FTEMP values is what is reported for FET Temperature since there are sometimes multiple temperature sensors in use. If FTEMP is 1, then it will average all of the temperature sensor readings and report the average. If it is 0, it will report the maximum value of all of the temperature sensors and report that for FET temperature.

    Regards,

    Anthony Baldino