This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61178: Design Questions

Part Number: TPS61178


Tool/software:

Hello Team,

Currently my customer is using TPS61178 in system and meet one design question, could you please help on it? Thanks!

The TPS61178 is connected to a 1V/5.5V power rail(The voltage may change between 1V or 5.5V in different board bring ups), which is powered before the TPS61178 output is enabled. The 1V/5.5V rail is connected by a diode and 1kOhm resistor to the TPS61178 output 12V, and the 1V/5.5V will power down when the TPS61178 output is enable. 

We want to check with you if any risk of this design. Thanks!

Regards,
Qiang