Other Parts Discussed in Thread: TPS922055, TPS922053, TPS922052, TPS922054
Tool/software:
I have measured the following undesired phenomenon on a TPS922055DMTREVM evaluation board, where the 1A output current is modulated with 2,1 kHz. I have changed the sense resistor to 200 mOhm (1A) and the inductor from 10 uH (10) to 100 uH (1,53A).
The goal is to have a very low ripple current through the LEDs, and eventually use analog dimming over the full 1:256 range.
Magenta is the LED current measured with a 50 MHz current probe, pink is the FFT from 0 - 10 kHz showing the frequency of the ripple as a peak at 2,1 kHz. Blue is the ADIM voltage (constant 3,3V).
What can cause the 2,1 kHz ripple? I thought it might be the COMP setting, but also thought that it would only have higher frequency effects. Is my assumption correct?

Any help in resolving the low frequency ripple will be highly appreciated.