This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5860: Max VIO_EN current

Part Number: LP5860

Tool/software:

Page 7 of the datasheet indicates that the maximum input current on V_VIO is I_VIO=5 uA.  This is stated under "Inteface Idle" test conditions.

What is the maximum current required for when the SPI bus is active?  I assume this will scale with the speed used, so let's assume worst case is 12 MHz SPI.

thanks!

-Steve