This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24192: Charge Termination

Part Number: BQ24192
Other Parts Discussed in Thread: BQ25628, BQ25622

Tool/software:

We are in the process of evaluating a new model using BQ24192 and are experiencing the following problem.

<Problem>
The Charge Termination Current is set to 128 mA, but the results vary greatly from 150 to 200 mA.
(Termination Current=128mA Charge Current=1024mA)

There is a large deviation from the ±20% accuracy in the specifications. Please provide possible reasons for the discrepancy.

Regards,
Kagawa