This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ79616-Q1: Power Regulator Failure

Part Number: BQ79616-Q1
Other Parts Discussed in Thread: BQ79616

Tool/software:

We have experienced an odd and so far unexplainable failure with one of our production Satellite BMS boards utilizing the Ti BQ79616 chip. The failure appears to be related to the power reuglation circuit and specifically the capacitor C302 in the attached schematic. There was no notable event when the failure occured. The board was in a shutdown state and had been sitting idle for several weeks. When the system was started up, this board failed to communicate and the decision was made to remove the battery from the vehicle in question. Upon inspection, the board was noticeably hot even in its shutdown state. The power regulator was reading 13-14 degrees with an infrared thermometer and the capacitor was measuring over 200 degrees. The input voltage to the regulator was 64V and the output was 3.85V. Unplugging the battery stack from the board and re-plugging it in had no affect. The chips immediately started to heat up again. The components are not under spec'd and this seems to be the only failure of this kind we have had. Are there any known reasons why this could happen or may have happened? Any input would be appreciated.

Here are the part numbers for the power regulation circuit components:

Ref Description MPN
C302 CAP, CERM, 1uF, 100V, +/- 10%, X7R, 1210 C1210X105K101T
Q301 TRANS NPN 150V 1A TO252 ZXTN4004KTC
R317 RES, 200 OHM, 1%, 2010, SMD RMCP2010FT200R
R318 RES, 100 OHM, 1%, 2010, SMD RMCP2010FT100R
  • Blakely,

    I suspect there is a short somewhere that is causing it to overheat. There are three likely candidates (in order of likelyhood):

    1) The capacitor shown in the image could be damaged or defective. Check the capacitance and continuity of this part and compare it to a working device.

    2) The BJT shown in the image could be damaged or defective. Check the continuity of this part.

    3) During shutdown, a short formed somewhere in the system. Check the continuity of the whole system.

    Since this is a problem in only one device, this single bad part is a likely explanation.

    Regards,

    Ben