Other Parts Discussed in Thread: LM5122
Tool/software:
Good Morning
We are testing a board where we used a LM5123-Q1 to boost UP an input voltage in the range of 9.5V - 16.0V to 11.9V. The input voltage will be, in normal operation, higher than the output boost voltage, so our idea was to use the chip in bypass mode most of the time and use it only when the input voltage drops down. The maximum continuous output current is 3.5A. In this test the enable pin is connected directly to the input voltage with a wire. We added a capacitor 1uF 0805 50V in parallel to C64 to add more capacitance at the bias input.
The schematic is this:
The boost, when the voltage is lower than 11.9V, work correctly as boost, realizing the correct output voltage at different load.
When we rise the input voltage over the output set point, it correctly stop switching and active the charge pump, in order to keep the high side mosfet high. and it correctly does it.
The problem appears when, from a voltage higher than 13V, we decrease linearly the voltage, at around 12.6V, the high side is turned off without any reason.
We checked both VCC and HB-SW voltage, and they are still high in this events; then there are two scenarios:
- if we continue to decrease the input voltage, at around 12.4V the high side is turned on again (with some pulse of switching);
- if we rise again the voltage, the high side is turned on again at around 13.4V;
Do you have any suggest or idea to solve this issue? Are we missing something in the operation of the chip?
Thank you very much in advance for help
Attached also a oscilloscope view: (CH1: high side gate, CH2: output voltage, CH3: VCC, CH4: not connected, all voltages are refer to ground)