Other Parts Discussed in Thread: HD3SS3212, TPS25730, TPS25751
Tool/software:
Currently I am trying to make the following: I have a DFP device which connects to my UFP port of a hub on my PCB via a USB-C Connector. With the HD3SS3220 i set its CC pins pulled down to indicate it is a UFP and I multiplex the SS lines. Besides this, I also connect a powerbank (supporting USBPD) to the CC pins of the device. This because my device needs to negotiate with the powerbank to let it give him 12V. So the device is DFP (Datawise) and UFP ( Powerwise)
My question is, will this work, since I connect CC lines from device to HD3SS3220 and to powerbank. The HD3SS3220 doesnt need to do anything with PD communication.
Thanks in advance.