Tool/software:
Dear sir,
We set the parameters according to SLUA792 when the sensor resistance is changed by a calibration ration of 20x (from 1m Ohm to 20m Ohm).
SLUA792 states "Parameters with units of mA, mW or mAh should be multiplied by the calibration ratio accordingly.".
For the BQ27Z561-R2, the following parameters are considered candidates. (refer to sluuc54c)
No. Address / Class / Subclass / Name
1. 0x4645 / Settings / BTP / Init Discharge Set
2. 0x4647 / Settings / BTP / Init Charge Set
3. 0x46CD / Advanced Charge Algorithm / Pre-Charging / Current
4. 0x46CF / Advanced Charge Algorithm / Maintenance Charging / Current
5. 0x4713 / Advanced Charge Algorithm / Termination Config / Charge Term Taper Current
6. 0x4721 / Gas Gauging / Current Thresholds / Dsg Current Threshold
7. 0x4723 / Gas Gauging / Current Thresholds / Chg Current Threshold
8. 0x4725 / Gas Gauging / Current Thresholds / Quit Current
9. 0x4663 / Gas Gauging / Max Load / Max Load Current
10. 0x4666 / Gas Gauging / Design / Design Capacity mAh
11. 0x4668 / Gas Gauging / Design / Design Capacity cWh
12. 0x4186 / Gas Gauging / State / Qmax Cell 1
13. 0x418F / Gas Gauging / State / Current at EoC
14. 0x4191 / Gas Gauging / State / Avg I Last Run
15. 0x4193 / Gas Gauging / State / Avg P Last Run
16. 0x419B / Gas Gauging / State / Max Avg I Last Run
17. 0x419D / Gas Gauging / State / Max Avg P Last Run
18. 0x465B / Power / Sleep / Sleep Current
--------------------------------------------------------------------------------------------------------------------------------------
19. 0x46AF / Advanced Charge Algorithm / Low Temp Charging / Current Low
20. 0x46B1 / Advanced Charge Algorithm / Low Temp Charging / Current Med
21. 0x46B3 / Advanced Charge Algorithm / Low Temp Charging / Current High
22. 0x46B5 / Advanced Charge Algorithm / Standard Temp Low Charging / Current Low
23. 0x46B7 / Advanced Charge Algorithm / Standard Temp Low Charging / Current Med
24. 0x46B9 / Advanced Charge Algorithm / Standard Temp Low Charging / Current High
25. 0x46BB / Advanced Charge Algorithm / Standard Temp High Charging / Current Low
26. 0x46BD / Advanced Charge Algorithm / Standard Temp High Charging / Current Med
27. 0x46BF / Advanced Charge Algorithm / Standard Temp High Charging / Current High
28. 0x46C1 / Advanced Charge Algorithm / High Temp Charging / Current Low
29. 0x46C3 / Advanced Charge Algorithm / High Temp Charging / Current Med
30. 0x46C5 / Advanced Charge Algorithm / High Temp Charging / Current High
31. 0x46C7 / Advanced Charge Algorithm / Rec Temp Charging / Current Low
32. 0x46C9 / Advanced Charge Algorithm / Rec Temp Charging / Current Med
33. 0x46CB / Advanced Charge Algorithm / Rec Temp Charging / Current High
--------------------------------------------------------------------------------------------------------------------------------------
34. 0x4691 / Gas Gauging / IT Cfg / User Rate-mA
35. 0x4693 / Gas Gauging / IT Cfg / User Rate-cW
36. 0x4695 / Gas Gauging / IT Cfg / Reserve Cap-mAh
37. 0x4697 / Gas Gauging / IT Cfg / Reserve Cap-cWh
38. 0x4660 / Power / Sleep / Deep Sleep Current
39. 0x4206 / Lifetimes / Current / Max Charge Current
40. 0x4208 / Lifetimes / Current / Max Discharge Current
41. 0x420A / Lifetimes / Current / Max Avg Dsg Current
42. 0x420C / Lifetimes / Current / Max Avg Dsg Power
Parameters No.1 to No.18 are changed to those setting value of 20 times.
The settings of parameters No.19 to No.33 are not changed.
Because, for example No.23. 0x46B7 / Advanced Charge Algorithm / Standard Temp Low Charging / Current Med's default value is 4004 mA.
This value by 20 times will exceed the set range (from 0 to 32767).
Parameters No.34 to No.42 are not changed as their default values are 0.
Are those settings correct?
Are there any parameters that do not need to be changed?
And, are there any other parameters that need to changed?
Best Regards,