This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62442: dual phase operation possible?

Part Number: TPS62442

Tool/software:

Hello,

as I'm planning to use TPS62442 as a dual output step-down converter, I was thinking of using the same regulator in the same project in a dual phase configuration to provide more output current (4A) by "shorting" both output channels as in the attached picture and using only one resistor divider to connect to both feedback pins (green: new connections, red: removed).



Is there anything I should be aware of when using the regulator in a dual phase configuration, or would you not recommend using the regulator in this mode?

Many thanks in advance