This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R2: Please helps to identify the most appropriate chip selection

Part Number: BQ40Z50-R2
Other Parts Discussed in Thread: BQ40Z50

Tool/software:

Hi Tier

Please help recommend the charge management chip, the requirements are as follows:
1, the input voltage range is minimum 5 ~ 30V
2, supports two kinds of battery charging, two "3S 18650 battery packs" charging, or two "4S2P 18650 battery packs" charging
3, the charging current supports software adjustment.
4, the maximum charging current is not less than 3A
5, support charging information reading, such as battery overcharge, battery failure, etc.

Is the BQ40Z50 the most suitable product ? Thank you very much!