This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi there!! As I have no previous experience with switching voltage converter ICs, I'd like to ask if there are any special precautions to be taken in order to power hifi audio equipment.
I plan to use a 10uF/10v MLCC ceramic (0805) cap (for C1) and to further minimise the power supply footprint
a few 47u/10V 0805 MLCCs. Also a 680uH choke from the output of the chip to the rest of the circuit. Are there any inrush current issues?
Any precautions during startup or power off?
Do I need to put any flyback diode in parallel with the choke? Are there any voltage spikes regarding the IC operation?
I have attached a quick schematic of what I plan to do. Let me know if there are any issues that I have to be aware of.
Hi
there maybe inrush current issues, because you add so many capacitance at the vout. Could I ask what the choke used for?
Thanks for your input! The purpose of the choke is to eliminate any switching frequency noise that may spread to the rest of the circuit. Do you think that my configuration could be harmful to the IC? The load circuit draws about 6-8mA @6V max.
Apart from the IC, do you think that the rest of the circuit is in potential failure risk, due to the above power supply configuration?