Tool/software:
Hi team,
Could you help check the schematic as below and any need to improve?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Zoe,
EN pin rising threshold is 1.2 (typical) and maximum is 1.27V so the mentioned Active UVLO range of 3.36 to 3.8V may not actually turn on the device. (Assuming this range is for Vin pin). It will be best for V_usb to remain greater than 4.14V for the device to turn on.
Other than this, I don't see any other issues.
Please click resolved if this answers your question or reply here with follow up question.
Best Regards.
Arush