Tool/software:
Hi,
1) Without PMBus
In my Board , I've designed TPSM846C23 power module to get 0.8V output. In Datasheet mentioned that, it is possible to operate the module without the need for a PMBus interface. To set the output voltage, the adjustment method requires a resistor, RSET, connected between the FB pin and AGND . But while im testing board i couldn't get desired output. i removed all pullup resistors and given 3.3V pullup for CNTL pin. But still get output
Here i'll attach my design schematics.

2)With PMBus
I've used Aardvark i2c mode, i can communicate with TPSM846C23 ,i tried updating the OPERATION register to 80h and ON_OFF_CONFIG to 00h (able to access the registers using Aardvark tool), but that also not giving any output. Please help me to resolve this asap.
Regards,
SUMAN