Tool/software:
hi expert
when i use 5V to supply UCC5871 VCC1. whether can i set UVLO1_LEVEL=0x0 and set OVLO1_LEVEL=0x0 at the same time?
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
hi expert
when i use 5V to supply UCC5871 VCC1. whether can i set UVLO1_LEVEL=0x0 and set OVLO1_LEVEL=0x0 at the same time?
thanks
Hi Jay,
Yes, you can select both as 0x0 but the demerit is the UVLO for 5V will be way lower now (2.45), hence the GDIC will function even when VCC1 fluctuates and goes as low as 2.5V for a 5V VCC1 (given everything else is powered up and working well). If that is something the customer is okay with, they can set both as 0x0.
Best,
Pratik