Tool/software:
So, I am trying to use the TLVM23625 part to generate a 1V power rail. I have already found that the datasheet to this part is wrong for the recommended feedback configuration to generate 1V and have already put Rfbt = 0 Ohm and RFBB = Open. I have attached a wire to confirm that I am receiving a power good signal from the part. The only differences I can find in my physical layout are that the two SW pins are tied together on the board.
I have attached my schematic for the setup of my TLVM23625.