This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS5430: Buck regulator suggestions

Part Number: TPS5430


Tool/software:

Hello,

We are planning to use 24V to 5V, 1.5A(min), buck regulator in one of our designs.

I have one general query as below:

As this is new design, which TI buck regulator part is suitable to use which has good market availability and minimum 10 years of EOL?

P.S. Above part# in tile is randomly selected, and it has very high current rating(3A) than we actually require.

Regards,

Nikhil Jadhav