Part Number: BQ25756EVM
Other Parts Discussed in Thread: USB2ANY,
Tool/software:
Hi,
I am having an issue with the USB2ANY first is I am unable to read any of the registers from the BQ25757EVM module
See below image, the BQ25756EVM schematics have J4 listed as the connector USB2ANY I2C interface, can you confirm if the USB2ANY is suitable for communicating with the BQ25756EVM noting that this module isn't explicitly listed as a compatible device. See Images below.

Secondly the USB2ANY Device seems to be somewhat unstable, remains powered but continually disconnects from the PC and loses communication with the USB2ANY Explorer 2.8.2 software.
has this been a problem in the past and if so, is there a solution available for it?
Cheers,
Jarred