Tool/software:
Hi expert,
In mass production, the E-FUSE used for 24V experienced a surge current and tripped during power startup, and the retry function (RETRY) could not function properly and could not be restored afterwards.
The trip current threshold set now is 7A, but the current during trip is 6A.
Even if a jump occurs, the inrush current should only flow once during startup, and then it should be able to be restored through the retry function, but it cannot be restored normally.
May I ask what factors caused this phenomenon to occur?
Thanks & Best Regards
bao