Other Parts Discussed in Thread: EV2400, BQSTUDIO
Tool/software:
I am working with the BQ40z50EVM and have followed the steps in the user guide to set it up. Here are the steps I’ve taken:
- Connected 4 batteries (ICR18650 3.7V 2500mAh) in series.
- Connected the power supply to PACK+/PACK-.
- Connected the serial communication port to the EV2400.
- Downloaded the bqStudio software.
- Connected the System-present pin to PACK-.
- Changed the DA register to set up the number of series cells to 4.
- Verified communication with the device.
- Set up the chemistry screen.
Despite following these steps, the BQ40z50EVM does not output voltage when a load is connected, and there is no indication that the chip is charging.
Could someone help me troubleshoot this issue? What could be the potential causes and solutions for the chip not outputting voltage or indicating charging?