Tool/software:
Hello!
We use your company's TPS27100 chip to test the load capacity with the output connected to the load. When ILIM is connected to the ground, the working environment temperature is 25 degrees Celsius and the load is 3.7A, the chip has the phenomenon that the protection is turned off and on again, and the switch continues.
The current limit 6A on the specification book, ask how to achieve the load capacity that can reach 6A.