This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ51050B: Wireless charging solutions

Guru 12815 points
Part Number: BQ51050B
Other Parts Discussed in Thread: BQ25170, BQ25100, BQ51003, BQ25180, BQ25120, BQ25155, TIDA-00318

Tool/software:

Hi,

Q1.
As far as TI's lineup is concerned, the only charger IC that supports wireless charging is the bq5105x. When selecting an IC, it is not necessary to be "Qi-Compliant," and the most important thing is to make the system compact. Are there any charger ICs other than the bq5105x that you can suggest?

The target battery is a 1-cell coin battery.
https://www.powerstream.com/p/Lir1620.pdf

Other companies seem to offer solutions for mobile applications for coin batteries that can be charged via NFC. I would like to know if there are any similar products.

Q2.
We are also considering a system that charges the above 1-cell coin battery via USB rather than wirelessly. BQ25170 and others seem to be applicable, but the following specifications are required.
-Power pass-through
-Ship mode (a function that prevents the coin battery from being depleted as much as possible when shipped)

Are there any products that you can suggest?

Thanks,

Conor