Other Parts Discussed in Thread: UCC28951, UCD3138
Tool/software:
Dear TI authority!
We are currently designing one power supply which can handle Bi-Directional Power Flow,
Specification for
Buck mode:
Primary: Input Voltage: 370VDC @ 3.4kW
Secondary: Output Voltage: 48VDC @ 50A
Boost mode:
Secondary: Input Voltage: 37-48VDC
Primary: Output Voltage: 370 VDC @ 3.4kW
We are considered to use UCC28950 in PSFB mode for Buck mode in converter.
Boost mode will be achieved by microcontroller and keeping disable UCC28950 IC.
(PFA reference circuit created by power designer!)
We will like to keep out modified design decision taken confirm/review by ti team!
Queries:
1. Do you have any application note which describe how to calculate transformer related details? (Like Windings, core structure etc.)
2. For L1 is it ok to use TMCS1127B1AQDVGR like IC with appropriate ratting?

Please let me know if you require any more details on this?
Best regards!
Umang Butani