Other Parts Discussed in Thread: LM5012, LM5013-Q1
Tool/software:
Good Morning everybody,
I have an issue with the LM5012-Q1 converter. For context we have a 12S-50V battery as a source for the converter and we are converting it to a 38V exit. We are observing an unexpected behaviour of the component : the output of the circuit is linked to a dc load to control the output current. Without any current, the buck converter outputs the expected 38V. But as soon as we increase the output current, we are observing a voltage drop. This drop continues until we reach a load of 1.3Amps and 30V. If we keep increasing the current, the voltage drops to 4.4V.
Simultaneously, we can hear a buzzing sound that might be coming from the LM5012. There is no overheating during the test detailed previously (checked with thermal camera).
Once the voltage drops to 4.4V, we need to decrease the load current to around 0.3Amps to suddenly get back to a "normal" voltage (of around 37V, so still off the supposed 38V). We have no idea where this hysteresis comes from.
Do you have any clue to what's happening there ? We cannot seem to find any description or explanation for the observed behaviour.
Attached are the schematic of the circuit used along with the LM5012 Q1 buck converter, as well as the pcb layout.
Thank you for your help and understanding.