Other Parts Discussed in Thread: BQ25790
Tool/software:
1,How can I determine the functionality of pin ILIM about being used as current limit setting or input current monitor, how to select between these two functionalites?
That's to say what can I do to select ILIM pin as input current limit setting or as input current monitor?
2,Regarding the " 9.2.12 Input Current Limit on ILIM" in BQ25890 datasheet, the voltage on ILIM pin can be 0.8V, 0.4V or others, so how does this voltage on ILIM come out and how can I decide what voltage on this pin,namely when the voltage is 0.8V and when the voltage is 0.4V?
3, When ICO_EN = 1, what's the relationship between IDPM_LIM register and IILIM register? And is ICO input current limit from IDPM_LIM register or from IILIM register now?
4, What's the difference between the condition V(BAT) < VMINSYS and V(BAT) > VMINSYS for ICO operation and how to understand this?
5, The charger must go into VinDPM once before ICO but why does the datasheet say " The device provides innovative Input Current Optimizer (ICO) to identify maximum power point without overload
the input source" ? Is VinDPM once not regarded as overload the input source?