Tool/software:
I am working with the UCD90160A part and have configured 12 rails with no inter-dependency between the rails. All are individual rails sequenced from 1 to 12.
I am now trying to use the "Pin-Selected Rail States" feature to define the rail status based on 3 different GPI pins.
From the Fusion GUI, under the configure menu and Rail #1-#12 configuration, I clicked on "Click to change PSRS" option in the Sequencing->How to turn rail on/off window and defined the states as shown below.
When I set the GPI1-3 pin states, I don't see the expected behavior.
My use case is the following:
1. GPI1-3 : ON/OFF/OFF - All Rails OFF
2. GPI1-3 : OFF/ON/OFF - All rails ON. (Expect rails to be re-sequenced and turned on, if they are already off).
Please confirm my understanding if this use-case can be achieved with the pin-selected rail states feature.