This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76905: Query for BQ76905 parameters configuration

Part Number: BQ76905


Tool/software:

we design win BQ76905. And there are some technical questions from customer. can you help to support that?

(1)the following picture is customer internal test item and criterion for 4cells system. They wanna confirm what can be programed at the factory and what can’t be programed and is constant?  The following criterion is for 4cells system of MP products, BQ79605 is used for 3cells new project.

(2)customer’s pack is 3S cells. Need BQ76905’s over discharge protection voltage point sets as 100mv, and charge protection voltage point sets as 20mv. if BQ79605 can be programed

 

  • Hi Harry,

    the following picture is customer internal test item and criterion for 4cells system. They wanna confirm what can be programed at the factory and what can’t be programed and is constant?  The following criterion is for 4cells system of MP products, BQ79605 is used for 3cells new project.

    The protections settings can be re-programed by an MCU. These settings do not persist between device resets and would need to be re-programmed again in the event of a reset. The list of programmable settings is available in the device's TRM: https://www.ti.com/lit/ug/sluuci8/sluuci8.pdf

    customer’s pack is 3S cells. Need BQ76905’s over discharge protection voltage point sets as 100mv, and charge protection voltage point sets as 20mv. if BQ79605 can be programed

    The OV protection is programmable from 0 to 5.5V in 1mV steps. The UV protection is programmable from 0 to 5.5V is 1mV steps as well.

    Regards,

    Max Verboncoeur

  • Hi Maxwell

    Thanks for your answer.

    1. All protections can be-programed in the OTP memory in factory as customer's requirement?

    2. How customer assesses the accuracy of protection configuration, what's the error between protection point actually and configured point

  • Hi Harry,

    All protections can be-programed in the OTP memory in factory as customer's requirement?

    It can be, although it would require a significant business case.

    How customer assesses the accuracy of protection configuration, what's the error between protection point actually and configured point

    The cell voltage protection accuracy is the same as the ADC measurement accuracy. The current protection accuracies are listed separately. You can find all of the specs in Section 6 of the datasheet.

    Regards,

    Max Verboncoeur

  • Hi Maxwell

    customer uses the free sample to build some prototype, and found there is not CHG and DSG driver signal. The schematic is shown as following picture. there are 3cells in system, we added a 9.6V input to simulate the battery.  

    if the default mode of BQ76905 is sleep mode? how convert the work mode from sleep mode to normal mode if there is no MCU in system?

    and if there is way that I can program the OTP memory on customer side to fix the parameter of BQ76905?

  • Add the register value

  • Hi Harry,

    The AFE by default allows entering SLEEP mode. Do you have the customer's .gg export file?

    Regards,

    Max Verboncoeur