This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25758: spec check

Part Number: BQ25758
Other Parts Discussed in Thread: BQ25756

Tool/software:

Hi

Is it possible to meet the following conditions?

VIN 4.5V ~ 36V

VOUT 5V/3A, 9V/3A, 12V/3A, 15V/3A, 20V/3.25

  • Hello Gareth,

    Yes, the BQ25758 can meet those conditions.

    We have a bidirectional USB-PD type C reference design that uses the BQ25756 that may help you. The BQ25758 and BQ25756 are very similar ICs. https://www.ti.com/tool/PMP41062

    Have you decided on a USB-PD controller yet? I can loop in USB-PD experts if you'd like.

    Let me know if you have any questions about this.

    Best Regards,
    Ethan Galloway