This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV61048: TLV61048DBVR

Part Number: TLV61048


Tool/software:

Can you please tell me what will be the max rated power of the part 

TLV61048DBVR
  • Hi Divyaa,

    I'm not sure about the max rated power you mentioned,

    If you are referring about the output power, it can be calculated with input voltage multiply current limit(avg) multiply 0.8. such as 2V*3A*0.8=4.8W

    If you are referring to the dissipate power, it is highly related to the layout, usually we consider 0.5W as its max dissipate power.

    Best Regards,

    Fergus