Part Number: TPS2552-1
Tool/software:
Hi,
I'd like to ask about the Figure.15 "Current Limit Response - μs" on page 10 of TPS2552-1 D/S as follows.

1. Regarding at the red circle, does this point mean that TPS2552-1 limit the current around 5A in 1.2 or 1.3us after Vout became short to GND?
(as an average data from multiple devices' test with VIN=5V, RILIM=20kΩ, TA=25℃)
2. Regarding at the blue circle, does this point mean that TPS2552-1 limit the current around 2.2A in 10us after Vout became short to GND (as an average data from multiple devices' test)?
(as an average data from multiple devices' test with VIN=5V, RILIM=20kΩ, TA=25℃)
3.Regarding the peak current at the red circle(about 5A), Is there any possibilities that the peak current would be the cause of the damage to TPS2552-1?
4.Do you have same type of data (means Figure 15) with the following conditions, VIN=5V, RILIM=47kΩ, TA=25℃?
Thanks,
Go