Other Parts Discussed in Thread: LM5160, UCC28701
Tool/software:
Hello,
I'm designing a phase-shifted full bridge DC/DC converter (18-50V to 28V @ 10A) controlled by the UCC28950. The schematic is based on the one we find in the datasheet of the controller ( UCC28950 Green Phase-Shifted Full-Bridge Controller With Synchronous Rectification datasheet (Rev. D)) but I have 2 questions :
- There's no explanations on how we can provide the 12V bias supply for powering the controller. Can I use the LM5160 controller in a buck converter, in order to get the 12V ?
- In the feedback loop, the output voltage seems to be directly connected to the controller (in the EA- for example). Is that normal given the fact that we are designing an isolated converter ? Or shall I add an isolated ampliop to achieve the isolation ?
Thanks in advance,
Regards,
Florian Wallaert