This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ2947: compared with BQ2945xy

Part Number: BQ2947
Other Parts Discussed in Thread: BQ2945

Tool/software:

Hi team,

What is the different between BQ2947 and BQ2945xy?

For 2 cells pack, BQ2947 and BQ2945xy, which do you recommend and why? The OVP is expected > 4.45.

  • Hello Kailun,

    The biggest difference is the number of cells of each. BQ2947 is 2s to 4s, BQ2945 is 2s to 3s.

    Both versions have OVP available for >4.45.

    The BQ2947 has higher tolerance for differential voltages between the VCx pins.

    Best Regards,

    Luis Hernandez Salomon