This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMG1210EVM-012: Heating Issue with LMG1210

Part Number: LMG1210EVM-012
Other Parts Discussed in Thread: LMG1210

Tool/software:

Hello.

I am using the LMG1210 to drive a full H- bridge, but it heats up when I apply a 5MHz PWM signal. For testing i set  supply voltages 10V DC, and the current is 500mA.I have attached the design files. Can you guide me to resolve this issue. Thanks

Best Regards.

Farhan

GATE DRIVER BOARD (21-03-2024 03-35-33).zip