Other Parts Discussed in Thread: TPS546D24S
Tool/software:
Hi team,
Could you help make sure that TPSM8S6C24 can support 3.3V I2C?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi team,
Could you help make sure that TPSM8S6C24 can support 3.3V I2C?
Hi Hale Tan
what do you mean by 3.3V I2C
TPSM8S6C24 module uses TPS546D24S IC and only support PMBus
Thank you
Savith
Savith,
Sorry about the mistake. Just want to make sure, whether TPSM8S6C24 can support 3.3V level voltage? Because the customers use GPIO in the MCU is 3.3V and they want to make sure whether need level shifter to change the voltage. I see that it can support. So just want to get confirmation.
Hi Hale
The CLK & DATA pins require pull up from 1.8 to 5.5V. Alternatively, the device uses the electrical specifications from PMBUS 1.3.
I would say 3.3V is okay
Thank you
Savith