Part Number: LM7480
Other Parts Discussed in Thread: LM5060, TPA3223, LM74912-Q1
Tool/software:
Hello all,
due to problems of the package type from the LM7480 i'm looking for the same functionality in a Pin-Package (SOP, SOIC, VSSOP, TSSOP .... everything except QFN/BGA/LLC).
The Part is used as a Powerpath controller with a inrush current controll. For sure it is possible to mimic the function with two different ICs. (e.g. LM5060 and LM74700x) but it would be prefereable to have it in just one package. Overcurrent Monitoring is not needed.
Are there any ideas here? Maybe there is some IC from TI which can perform this function or it is possible to use an LM5060 with a little additional circuitery here.
Working Voltage is 10-30V, Working Current up to 30Arms. Capacitive Load switched/driven: 3000µF
Thanks a lot!
Best regards,
Lukas