Tool/software:
Hi,
I've read the forum below and I have the same issue:
I believe Euan's question in the aforementioned forum was misunderstood.
I'm making an LLC converter from 48V to 24V with maximum load 6.25A, and to simplify the qualification process, I disabled burst mode which might be what's causing my issue.
The issue is that output voltage regulation is lost, the maximum switching frequency is at around 170 kHz, and it doesn't go any higher.
So, when Vin is 48V, and the load is lower than the maximum load (≈4.4 A), Vout goes above 24V (up to 28V), so the gain is too high but the controller can't increase the frequency anymore to bring the gain down.
So the question is:
What can be causing the maximum frequency to be limited to a certain value and not any higher?
How is that related to disabling burst mode?