This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7481-Q1: LM74810QDRRRQ1 how to reduce turn off time

Part Number: LM7481-Q1

Tool/software:

Dear Sir/Madam,
I am planning to use LM74810QDRRRQ1 to control a wiper motor. 
The turn on time is fine (6ms) however the turn off time needs to be reduced (553ms).
To park the motor the turn off time needs to be under 200ms.
I have attached some scope shots from the EVM for turn on and off.
GREEN= EN/UVLO pin
YELLOW=VOUT 
Motor current is 1.9A.

I was thinking about using a MOSFET load that is enabled when the LM74810QDRRRQ1 is disabled.
Not sure if this has been done on any TI EVMs.
Suggestions are welcome.

Regards Joe