Other Parts Discussed in Thread: UC3842
Tool/software:
Dear experts,
The flyback power supply input voltage is 24VDC ,Vout=16V and the input capacitor is 9 x 10uF MLCCs in parallel.
When the flyback power supply is loaded with 1A, the input voltage fluctuates violently PP-1.35V, and the yellow waveform is the input voltage ripple.
Why does the input voltage fluctuate with the increase of load, and how to calculate the value of the input capacitance with DC input.I find a calculation method in UC3842's datasheet but it calculate with a rectifier bridge
Thankyou