Tool/software:
Hi TI team,
There is no Aux widing, but to improve the customer board, the customer is reviewing the data sheet's application.
The circuit of the application is output 24V / 5V.
However, in the Flyback Transformer calculation formula, it is calculated with VOUT 19V.
1. Please explain why Vout1 is calculated as 19V.
2. If the application has an additional output of aux winding.
OUT1 : 18V
OUT2 : 6.7V
Aux OUT3 : 5.7V
Should I calculate it as Vout1 = 18V-6.7V-5.7V?