Tool/software:
Hi,
PSPICE
TPS7H4010-SEP_AVG : gives the expected output bias point (5V, 140mA) but the model should not be used for transient analysis => fails to achieve any line regulation (output rises to 6V).
TPS7H4010_TRANS PSPICE model seems not to work in my environement (PSPICE for TI). The output is stuck to 0V.
LTspice
For debug, the two SUBCKT files were read into LTspice. Both models (TPS7H4010-SEP_AVG ,TPS7H4010_TRANS) give a 5V,140mA output.
The startup transient of TPS7H4010_TRANS looks correct (ramp then stabilize).
However, a couple of warning doesn't give confidence that the simulation is actually correct.
Tina
The TPS7H4010_TRANS Tina model seems to work but is extremely slow (> 60s).
Best regards,
Vincent
Remark : I am new to PSPICE. I know well the cadence and LTspice environments