Tool/software:
Hello,
In the data sheet it says
"For better protection from a hard short-to-GND condition (when the ENx pins are enabled, a short to GND occurs
suddenly), the device implements a fast-trip protection to turn off the related channel before the current-limit
closed loop is set up. The fast-trip response time is less than 1 μs, typically. With this fast response, the device
can achieve better inrush current-suppression performance."
So at some current value it decides that there is a hard short circuit and initiates the fast-trip protection.
Q1 At what current does the fast-trip protection take over form the current limit function ?
Q2:What is the maximum short circuit current the device can take without damage ?
Reason is that on a hard short circuit test with a 24 V 14 A power supply unit the device failed as shown below
Best Regards,
Chris