Other Parts Discussed in Thread: LMR51606
Tool/software:
Hi,
We are going to use LMR51610 and we have these specifications:
Vin = 9-30V
Vout = 3.3V
Iout = 0.25A
Fsw = 400kHz
When we use the Webench tool, we are getting L = 18uH-22uH which means a input ripple 130%. It is common to select 20%-40%. Why did the tool select such value? Additionally, we know the boundary for CCM and DCM in a buck converter is:
2L/(R*Ts) = (1-D), Rcrit = 2L/(1-D)Ts. For L = 150uH, Rcrit = 134.8ohms and L = 18uH, Rcrit = 16.18ohms
so the higher the inductor, higher the range of R which the converter can work in CCM. However, when I simulated the circuit in PSPICE for TI, it showed me higher the inductor, it is more likely the system works at DCM. Furthermore, I was expecting a decline in the ripple between the two values, but it doesn't have any major change
Full load L 18uH (R = 13.2):

Half-load 18uH(R = 33)
Full load 150uH(R = 13.2)
Half-load 150uH (R = 33)