This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25947: Lower than expected ILM in negative supply rail configuration

Part Number: TPS25947

Tool/software:

Hi,

I am using a TPS2594EVM board to create an overcurrent protection circuit for a pair of power supplies connected in series.

When the kit operates in a single power rail condition, it trips at the current I set, at which point the voltage on Pin-9 (ILM) is about 0.61 V with repect to the local ground.

However, as soon as I connect the negative end of the protected positive output (V_out_pos-) to the positive end of the protected negative output (V_out_neg+), the voltage at Pin-9 of the negative TPS25947 would become much lower than expected. Therefore, it would require a much higher current to trip the negative rail. I am wondering what is causing the problem. 

Here are some of my test data:

Given RILM of 1.65 kohms, at load current of 2.0 A:

Single supply: Vilm = 0.604V, (which make sense, because 182e-6 uA/A * 2.0 A * 1650 ohm = 0.600V)

Negative supply: Vilm = 0.228V

When the two protected outputs are not connected, there is a +25mV between V_out_pos- and V_out_neg+.

Also, how does the device sense the current going through the FETs?

Thank you!