This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51375: Designing Problems about TPS51375

Part Number: TPS51375

Tool/software:

Hello SR support team,

This is Dave supporting Industrial PC customers.

We have a new project designing the following spec.:

Vin:4.75V~20V

Vout:0.77V

TDC:7.6A

ICCMAX:15.2A

I found that our new product Hades (TPS51375) would be suitable.

But we have some question here:

Q1: Do we have the symbol file could provide to customer?

Q2: For the voltage spec., TPS51375 has the ability for 4.5V to 24V. However, why the ref design (EVM) only using 5.5V to 24V and avoid the common voltage of 5V input? Is there any reason?

Please kindly suggest, thanks.

Dave