Other Parts Discussed in Thread: UCC28070, UCC28019, PMP22606
Tool/software:
Hello Everyone,
I need Ucc28180 IC's Unencrypted lib file. If any one have kindly reply to me or give the tips where it located.
1. Actually, I'm making 800W - 1000W PFC circuit using UCC28180 IC in cadence, but what i'm facing the problem was i'm not getting the GATE pulse at the o/p of 8pin.
2. I agree, what are things available on ucc28180_AVG spice model in TI website and i'm calling both olb & lib files and BOOSTCCMDCM file also added.
I create a circuit what in available on reference and I am getting the PFC boosted 380V range o/p voltage. but my intension was i need Gate pulse signal in o/p of 8 pin.
3.In TI compony provides other CCM PFC IC's also i'm facing same problem.
4.I want to see the Gate pulse even any of this Ic ucc28180,ucc28019,ucc28070,ucc2806x series. Any possibilities are there?
Thanks Guys,
Regards
Suriya