This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65400-Q1: Schematic review

Part Number: TPS65400-Q1


Tool/software:

Hi,

Please help to review schematic, thanks

Vin 12V,

Vout1 1.8V 0.5A,

Vout2 1.1V 3A,

Vout3 3.3V 0.1A,

Vout4 disable

  • Hi Wen,

    My colleague Lucia will reply later.

    Thanks

    Colin

  • Hi Sir,

    From the schematic, the resistor (R68=100kohm), it means that the target switching frequency in theory is 1.761MHz and the target switching cycle is around 568ns. If we take 1.1Vout rail as an example, the typical Vin=12V. Thus the HS on time need to support 52ns in theory. However, you can find from our EC table that tonmin max value is 150ns. It will be a limitation for the lower duty cycle. We would recommend you can re-design the switching frequency to achieve lower duty cycle (max Vin to lowest Vout). After re-design the switching frequency, you can double check your inductor, Cout and compensation components value.

    Thank you.

    BRs

    Lucia